MITSUBISHI ELECTRIC Changes for the Better
Packaging

Packaging automation trends

28.08.20264 Minuten Lesedauer

Packaging is an important part of the manufacturing process. It protects products, prepares them for transport and supports handling throughout distribution. The process may include filling, forming, sealing, labelling, cutting, case packing, palletising and final preparation for distribution. When these operations are poorly coordinated, manufacturers may experience interruptions, inconsistent results and delays further down the production line. Packaging automation connects machines, control systems and handling equipment. Its purpose is to coordinate packaging operations and reduce the need for manual intervention in defined parts of the process. The latest packaging automation trends include robotics, integrated machine control, smart packaging systems and Industry 4.0 technologies. Together, they can support better production visibility and more coordinated packaging processes.

What is packaging automation?

Packaging automation is the use of machines, control systems, robotics and related technologies to perform or coordinate packaging operations.

It may cover a single stage, such as labelling or filling, or an entire packaging line. Typical applications include bottle filling, pouch packaging, forming, filling and sealing, case packing, palletising and product handling.

Manufacturers can use packaging solutions to connect different stages of the process and adapt automation to the requirements of a specific packaging application.

Automation can be used in primary, secondary and end-of-line packaging. Primary packaging comes into direct contact with the product. Secondary packaging groups products into cases or other units. End-of-line packaging automation prepares finished products for storage and distribution.

An automated packaging system may combine mechanical equipment, sensors, programmable controllers, drives, operator interfaces, robots and safety functions.

These components work according to defined sequences. For example, a system may detect a product, fill a container, apply a label and transfer it to a case-packing station.

The equipment must therefore work as part of a coordinated process. Packaging automation is not only the purchase of one machine. It also includes the communication and control architecture that connects the different stages.

Why packaging automation is transforming modern manufacturing

Packaging performance affects the wider manufacturing process. A problem in filling, labelling, case packing or palletising can limit the output of other machines.

When equipment operates independently, operators may need to adjust settings, transfer information, respond to faults or manage product changes manually. This can make the production flow more difficult to control.

Packaging line automation creates a more structured way to coordinate these activities. Machines can exchange status information and operate according to shared sequences.

This is particularly relevant when manufacturers work with several products or packaging formats. Each change may require different settings, handling conditions or machine sequences.

End-of-line operations are also important. If products are manufactured faster than they can be packed, grouped and palletised, the entire process is limited by the slowest stage.

For this reason, industrial packaging automation increasingly covers the complete flow from product handling to distribution preparation.

Automation also changes the role of operators. They can supervise equipment, respond to defined conditions and manage the process through control interfaces instead of carrying out every packaging task manually.

Human expertise remains necessary. Operators and engineers still need to understand the process, investigate interruptions, manage formats and maintain equipment.

  • Integrated packaging line automation

    One of the main packaging automation trends is the integration of equipment across the line.
    Filling, labelling, packing and palletising can be connected through a common automation structure. This allows machines to exchange information and operate according to shared sequences.
    Integration can also support troubleshooting. When a line interruption occurs, the system can help identify the affected process stage and its relationship with other equipment.
    A connected line is more than a group of machines placed next to one another. The equipment also needs to communicate and operate as part of the same process.

  • Flexible packaging equipment

    Manufacturers may need to change between products, pack sizes or packaging formats. This creates demand for packaging equipment automation that can support more than one configuration.
    Depending on the application, flexibility may involve adjustable settings, recipe management or controlled changeover sequences.
    The level of flexibility depends on the equipment and its design. A line may still require substantial manual work if every format change involves physical adjustments.
    Changeover requirements should therefore be considered at the beginning of the automation project.

  • Robotics in packaging

    Robotic packaging systems are used for repetitive operations such as product handling, grouping, case packing and palletising.
    A robotic application usually includes conveyors, product detection, grippers, control systems and safety equipment. The robot is one part of the complete packaging solution.
    Robotics are particularly relevant to end-of-line packaging automation. Products may be picked, arranged, placed into cases or stacked on pallets according to a defined pattern.
    The suitability of a robotic system depends on product characteristics, packaging format, product presentation, required flexibility and the surrounding equipment.

  • Smart packaging systems

    Smart packaging systems use connected control, monitoring and data exchange to make packaging operations more visible.
    The system may provide information about machine status, operating settings, active faults or production sequences. This information can support troubleshooting and process improvement.
    The value of a smart system depends on whether the data is accessible and useful to the people managing the line. Data collection alone does not improve production.

  • Industry 4.0 packaging

    Industry 4.0 packaging involves connected automation, digital control and data exchange within packaging operations.
    It may include communication between machines, centralised monitoring, structured fault information and connections with wider production systems.
    Manufacturers should first define what information they need and what decisions it should support. The purpose of Industry 4.0 integration is to improve visibility and coordination, not simply to collect more data.

How robotics and AI improve packaging production efficiency

Robotics and AI have different roles in packaging automation.

Robotics performs physical operations such as picking, placing, grouping, case packing and palletising. AI in packaging may support analysis, recognition or decision-making, depending on the application.

Automated case packing is one example of a robotic application. Products arrive on a conveyor, are detected and grouped according to a defined pattern before being placed into a case.

The complete process requires suitable product presentation, case handling, grippers and control logic. A robot alone does not create an automated case-packing system.

Palletising automation follows a similar principle. Cases or other units need to arrive in a controlled way before being placed according to a defined stacking pattern.

AI may be relevant where the packaging process includes a specific recognition or analysis task. Its usefulness depends on the quality of the data, the problem being addressed and the connection between the AI output and the production process.

Not every automated packaging system requires AI. Many systems operate through predefined parameters and control logic.

The most practical approach is to match each technology to a defined production requirement.

TechnologyTypical role in packaging
Control systemsCoordinate machines and operating sequences
RoboticsPerform defined handling, packing and palletising tasks
Monitoring systemsProvide information about status and faults
AISupport specific analysis or recognition applications

Smart packaging systems and Industry 4.0 integration

The control system coordinates machine sequences, communicates with equipment and allows operators to interact with the packaging line.

The Mitsubishi Electric materials describe machine solutions that include control platforms such as System Q and technologies used in machine automation.

A packaging system may need to manage motion control, sequencing, sensors, drives, operator interfaces, machine communication and safety-related functions.

When these elements are disconnected, diagnosing problems can be more difficult. An integrated system creates a clearer connection between the physical process and its control logic.

For example, if a product does not reach a filling station at the expected time, the cause may be related to a conveyor, sensor, preceding machine or control sequence. Communication between equipment can help engineers investigate the problem more systematically.

Recipe-based operation may also support lines that handle different products or formats. Operators can select a defined group of settings instead of entering every parameter manually.

Human-machine interfaces provide access to line status, alarms and permitted controls. Their usefulness depends on whether the information is presented clearly and in the context of the process.

Manufacturers may also connect packaging equipment with wider production, monitoring or maintenance systems. The appropriate level of integration depends on the existing factory architecture.

Benefits of packaging automation for manufacturers

Packaging automation can support more consistent process execution. Automated equipment follows defined sequences for operations such as filling, labelling, packing and palletising.

The result still depends on machine setup, maintenance, product characteristics, packaging materials and control parameters.

Connected equipment can also improve coordination. Machines exchange information about their status and can operate according to shared sequences.

Monitoring may help operators and engineers understand line conditions, active faults and interruptions. This can provide a basis for packaging process optimization.

Robotic systems can perform repetitive handling tasks that would otherwise require manual movement. Their suitability depends on the product, packaging format, operating speed, changeover requirements and safety conditions.

Automation may also make changeovers more structured through predefined settings, recipes and controlled sequences. The effect depends on the design of the packaging line.

Case packing and palletising connect final packaging operations with the wider production flow. This can help prevent end-of-line activities from becoming a separate bottleneck.

Sustainable packaging and the role of automation

Sustainable packaging automation involves using automation to support more controlled packaging processes and the use of materials and resources.

Automation does not make a process sustainable by itself. Sustainability depends on packaging materials, product design, transport requirements, energy use and waste levels.

Automated systems can support repeatable operation and controlled process parameters. This may be relevant to forming, filling, sealing, labelling and material handling.

Any claim about reduced material use, lower energy consumption or reduced waste should be supported by data from the specific production line.

Changes to packaging materials or formats can also affect the rest of the process. A different package may require adjustments to forming, filling, sealing, labelling or transport.

Sustainable packaging automation should therefore be assessed at system level. The key question is how automation can help manufacturers control a defined process and measure the outcome.

Choosing an approach to packaging manufacturing automation

There is no single automated packaging solution suitable for every manufacturer.

The right approach depends on the product, packaging format, production sequence, available space, changeover frequency, operator involvement and end-of-line requirements.

Before selecting equipment, manufacturers should map the current process. This includes examining product flow, packaging formation, filling, labelling, case packing and palletising.

It is also important to identify where operators intervene and where interruptions occur. These points can help define the requirements for the future system.

The control architecture should be considered together with the mechanical equipment. Controls, drives, sensors, interfaces and communication need to work as parts of one system.

The approach will also differ between a new line and the modernisation of an existing one. A new installation can be designed around one automation structure, while an existing line may require the connection of equipment from different generations.

A useful starting point is to review the available packing solutions and compare them with the requirements of the application.

Manufacturers may also consider how packaging automation fits into the wider factory. The example of a smart automotive factory illustrates the importance of connected automation, communication and production visibility.

The equipment should match the packaging task. A horizontal packaging machine addresses different requirements from a vertical form-fill-seal machine, bottle filling system or palletising cell.

Packaging automation across different applications

Packaging automation can be adapted to different packaging processes.

Bottle filling systems transfer products into bottles according to the defined filling process. The wider application may also include container handling, closure application, labelling and transfer to later stages.

Labelling systems apply labels to products or containers. Their integration with the rest of the line is important because product position, speed and detection affect the timing of the operation.

Horizontal and vertical pillow packaging machines form, fill and seal packaging in a defined sequence. A horizontal packaging machine may be used where the packaging process requires horizontal product handling and sealing. The appropriate configuration depends on the product and package format.

Vertical form-fill-seal systems create packaging from a roll of film, fill it with the product and seal the package. The process requires coordination between film movement, product dosing, forming, filling and sealing.

Rotary cutter applications use controlled cutting movements within the packaging process. Synchronisation between the cutter, product flow and surrounding equipment is important.

At the end of the line, case packing and palletising prepare products for handling and distribution. These operations may involve robots, conveyors, detection systems and defined stacking patterns.

Each application has different technical requirements. A packaging automation project should therefore begin with the operation to be performed rather than with a generic technology label.

FAQ section

What is packaging automation?

Packaging automation is the use of machines, control systems, robotics and related technologies to perform or coordinate packaging operations with limited manual intervention. It can cover individual activities such as filling, labelling or sealing, as well as complete processes including case packing, palletising and preparation for distribution.

How do automated packaging systems work?

Automated packaging systems use mechanical equipment, sensors, programmable controllers, drives, operator interfaces and, in some applications, robots. These components work according to defined sequences. The system detects products or packaging materials, performs the required operation and transfers the output to the next stage.

The exact configuration depends on the product, packaging format and process requirements.

What are the benefits of packaging automation?

Potential benefits include more consistent process execution, better coordination between machines, improved visibility of line status, support for repetitive handling and more structured changeovers. Automation can also connect primary packaging with secondary and end-of-line operations.

The actual benefits depend on the equipment, application and implementation.

How does packaging automation improve production efficiency?

Packaging automation can improve production efficiency by coordinating machines and reducing unnecessary manual intervention in defined processes. It can also help manufacturers monitor operating conditions, identify interruptions and connect end-of-line activities with the wider packaging flow.

The effect should be evaluated using data from the specific production line.

What industries use automated packaging systems?

Automated packaging systems can be used in manufacturing environments that involve processes such as bottle filling, labelling, pouch packaging, form-fill-seal operations, case packing or palletising. The suitability of a system depends on the product, packaging format, production process and required handling method.

How do robotics support packaging automation?

Robotics support packaging automation by performing defined physical tasks such as picking, placing, grouping, case packing and palletising. Robotic systems normally operate as part of a wider application that includes conveyors, product detection, grippers, control systems and safety functions.

Is packaging automation suitable for small and medium-sized manufacturers?

Packaging automation may be suitable for small and medium-sized manufacturers, depending on the process, production requirements, available space and expected level of flexibility. The appropriate solution may involve automating one stage of the process rather than the entire line.

The decision should be based on the specific operation and the manufacturer’s requirements.


Ähnliche Artikel


Themen

Packaging