MITSUBISHI ELECTRIC Changes for the Better

Hydraulic systems generate unnecessarily high energy costs in many production environments. Especially in presses, die-casting machines, and hydraulic power units, motors often run continuously at full speed regardless of the actual power demand.

With an intelligent retrofit solution consisting of frequency inverters, speed-controlled pump systems, and energy-efficient synchronous reluctance motor systems, energy consumption, heat losses, and operating costs can be significantly reduced.

Mitsubishi Electric frequency inverters achieve efficiencies of more than 98% and enable particularly low-loss operation. By dynamically adjusting motor speed to the actual load demand, typical energy savings between 20% and 50% can be achieved, depending on the application and load profile.

Why conventional hydraulic systems operate inefficiently

In many existing hydraulic systems, pump motors are often switched on via a contactor and run continuously at full speed. The actual load is then regulated using valves or throttling mechanisms. The excess energy is not utilized but converted into heat. This results in high thermal losses and additional energy demand for cooling systems or fans.

Typical problems:

  • High power losses caused by throttle valves
  • Overheating of the hydraulic oil
  • Continuous full-load operation
  • High power consumption during idle operation
  • Unnecessary heat generation
  • Increased cooling requirements

Especially in applications with fluctuating loads, a hydraulic retrofit offers significant energy-saving potential.

Saving energy through intelligent speed control

By using a frequency inverter, the speed of the hydraulic pump is precisely adjusted to the actual demand.

For example, when a hydraulic cylinder retracts or the application is operating in idle mode, the Mitsubishi Electric frequency inverter automatically reduces the speed or stops the motor completely.

Even a small reduction in speed can have a significant impact on power consumption:

  • 20% lower speed
  • Up to 50% reduced power consumption

Especially during idle operation of pumps or fans, this results in considerable energy savings.

Retrofit: hydraulic systems with frequency inverter

The combination of modern drive technology and intelligent control creates an energy-efficient overall solution.

Through speed-controlled operation of the hydraulic pump, performance is precisely adjusted to the actual demand. This results in significantly lower energy losses compared to conventional hydraulic systems with constantly running motors and throttle valves.

    Variable speed instead of continuous operation

    The pump operates only with the actually required power. During idle operation or reduced load demand, the speed is automatically reduced or the motor is stopped.

    Reduced heat losses

    As significantly less excess oil needs to be throttled through valves, thermal losses within the hydraulic system are greatly reduced. Less energy is converted into heat.

    Lower operating costs

    Reduced energy consumption lowers operating costs. At the same time, reduced heat generation decreases the cooling requirements of the system, resulting in lower energy demand for fans or external cooling systems.

    Reduced wear on components

    Lower thermal and mechanical stress increases the service life of hydraulic components, pumps, and hydraulic oil.

    Minimized reactive power

    With a power factor (cos φ) close to 1, no unnecessary reactive power is drawn from the supply grid during idle or partial-load operation. This reduces grid load and limits active power consumption to the actually required level.

    Fast integration into existing systems

    Retrofit instead of complete machine replacement – existing hydraulic systems can be efficiently modernized and optimized for energy efficiency.

    Typical applications for energy-efficient hydraulic systems

    Presses

    Load-dependent speed control reduces energy consumption during standby and partial-load operation.

    Die-casting machines

    Variable pump control prevents unnecessary full-load operation.

    Hydraulic power units

    Efficient pump control minimizes heat generation.

    Scissor lift and cylinder systems

    Demand-based power control improves system efficiency.

    SynRM motors for maximum energy efficiency in hydraulic systems

    In addition to intelligent speed control, the choice of motor also plays a crucial role in the energy efficiency of modern hydraulic systems. Synchronous reluctance motors (SynRM) have been specifically developed for highly efficient operation with frequency inverters and combine high energy efficiency with robust industrial performance.

    This results in several advantages:

    • High efficiency
    • Low rotor losses
    • Reduced heat generation
    • Compact design
    • Energy-efficient operation in partial-load conditions

    Especially in hydraulic applications with fluctuating loads and long operating times, this technology offers significant advantages over conventional induction motors.

    FAQ – Frequently asked questions about hydraulic retrofitting

    When is a frequency inverter worthwhile in hydraulic systems?

    The use of a frequency inverter is particularly worthwhile in hydraulic systems with fluctuating load profiles, frequent idle phases, or continuously running pump motors. Demand-based speed control can significantly reduce energy consumption depending on the application.

    What energy savings are possible with a hydraulic retrofit?

    The actual savings depend on the application, load profile, and operating times. In many hydraulic applications, typical energy savings between 20% and 50% can be achieved through speed-controlled pump systems and modern drive technology.

    Can an existing hydraulic system be retrofitted?

    Yes, many existing hydraulic systems can be efficiently retrofitted with frequency inverters and modern motor systems. This improves energy efficiency without the need to replace the entire machine.

    What are the advantages of a speed-controlled hydraulic pump?

    A speed-controlled hydraulic pump adjusts its performance precisely to the actual demand. As a result, energy consumption, heat generation, and mechanical stress are significantly reduced compared to conventional continuously running systems.

    What are the advantages of synchronous reluctance motor technology in hydraulic systems?

    SynRM motors offer high efficiency, reduced heat generation, and excellent efficiency in partial-load operation. In combination with Mitsubishi frequency inverters, they create a particularly energy-efficient overall system for modern hydraulic applications.

    Modernize hydraulic systems efficiently now

    Optimize existing hydraulic systems with intelligent speed control, modern drive technology, and energy-efficient motor systems. We will be happy to advise you. Contact us using the contact form and we will get back to you as soon as possible.

    The fields marked by a * are mandatory.